Hello all!
I’m trying to use the Sunny Buddy with two solar panels as described in the instructions.
I soldered a second barrel jack on, cleared J1 and bridged J2 which should connect the two solar panel jacks in series.
When I measure the output voltage of the disconnected solar panels, they each read about 7 volts in the sun. Plugging the first panel into the original barrel jack, I read the same voltage on the pcb.
However, when I plug in the second panel, I read around 5 volts from ground to the higher voltage potential of the second panel.
I thought I should be reading around 14 volts, since they are connected in series, but am I missing something?