Music Reactive LED Lighting Controller Demo powered by ESP32 and Arduino Core

Hey everyone, this is a demonstration of a music reactive LED lighting controller we’ve been developing!

Current status is a plug-and-play board that can be configured/controlled via smartphone. It supports basically any common LED strip you can find, the only thing you have to do is make sure to match the voltage inputto the board to the voltage the LED strips run at(usually 5v or 12v) . It is centered around an ESP-WROOM-32 module running Arduino Core which does all the sound processing, lighting control and handles the wifi/bluetooth. It should be able to control >1000leds and it can handle >8amps of current.

We would love any feedback/criticism you have regarding how it looks, suggestions for the future, or just general comments. The platform is pretty versatile at the moment so there are lots of places it can go! Thanks!