my first breakout board for Nokia's LCD - crits pleas!

Hi guys,

I tried to designing a simple breakout board for connecting an LCD from Nokia 6060/6010 to SPI of panda II.

http://s15.radikal.ru/i189/1105/dd/05dbb4bd7bd4.jpg

What do you think? In terms aren’t there any obvious mixups with the pins or such…

Thanks! :smiley:

Here’s the pinout for this LCD that I found here
http://rossum.posterous.com/screen-play … or-microco
1 VCC
2 LED+
3 GND
4 GND
5 SCLK
6 GND
7 GND
8 GND
9 GND
10 GND
11 -
12 RESET
13 CS
14 GND
15 GND
16 GND
17 GND
18 MOSI
19 GND
20 GND
21 VCC
22 LED-

I would add some bypass capacitors (at least a 100nF between Vcc and GND near the connector). I would also use wider traces for VCC, GND, and the LED ones.

Do you need any mounting holes?

/mike

The connections to the pads are off-centre, it looks a bit untidy.

I would add some bypass capacitors (at least a 100nF between Vcc and GND near the connector)

I'm kinda new to electronics, please explain, what for would this capacitors be?

I would also use wider traces for VCC, GND, and the LED ones.

Yes, I'll make all traces at least 0.7mm ( currently pads are 0.25mm ).

Do you need any mounting holes?

Yes, there would be holes and a connector like this:

http://web.argus.lv/shop/images/BL1X08L/hwindex.htm

The connections to the pads are off-centre, it looks a bit untidy.

It's just that way in the image. On the pcb it'll be nice and tidy. :)