I am getting absolutely nothing out of my Venus GPS-09133.
The situation:
The SPI pins are all floating (unconnected).
I have 3.3V verified on the board pins 3V3 and VBAT, as well as across the filter cap on the board.
I left IO1, IO2, and IO20 floating.
There is an LED on the board that is glowing exceedingly dimly (barely visible). The board seems to be drawing very little power according to my power supply (maybe 10-20 mA).
I am using the TTL-level serial connection, set on my end to 9600 baud. The TX line from my UART is connected to the RX input on the board, and vice-versa.
I have tried sending the board commands, but I get no ACK or NAK. I get no output from the board either.
I see no activity on the device’s TX pin. Both TX and RX are always 3.3V.
Am I doing something obviously wrong here?