It should have 0.1 inch pin spacing, with 3 leads and female ends on both sides. What is a term that works on Mouser to find it? I’ve tried “3 lead cable”, “0.1 3 lead cable”, and other things but nothing seems to work. I would like a picture to appear alongside the product as well so I can check, so none of the VCC cables are very helpful.
I don’t think they’ll have ready made cables like that, but maybe made to order. I think Digikey is the same. I’ve run across this with small pitch cables, even with a manufacturer part number.
I did find them at Parallax, but only in a kit, or a 68" version.