I am needing to add a button to a project, it is a kerchan sad0705k monitor and it has the ability to add buttons to it to control video playback. To get a button from them will cost me too much in shipping, they will not use anything but DHL. attached is the photo of the plugs, 4 connectors, would like to find a cable that would hook into this, so I can add a button to it. any ideas? thanks
It looks like the first two links are to connectors with 1.5mm pitch (~0.059 inch) and the last link is to a JST connector with a link to a JST datasheet that describes the pitch as 2mm (~0.079 inch).
ataripirate:
…attached is the photo of the plugs, 4 connectors, would like to find a cable that would hook into this, so I can add a button to it. any ideas? thanks
Can you recreate that photo with a ruler next to it for scale?
From your picture, the 2mm pitch looks to be correct. So when SparkFun gets more in that might be the one. Alternatively, Digi-Key sells the housing (455-1164-ND) and pins (455-2148-1-ND) but you would need to make up the cable yourself.