LPC-E2468 (P/N DEV-08854) NAND flash is not detected.
I have reinstalled U-Boot using FlashMagic, still same except build date (was Oct 08 2008 now Apr 15 2008 after reboot)
Flash is HY27UF081G2M, look under microscope no solder bridge on NAND nor on CPU.
my bad or defective board ?
**********************************************
* LPC-E2468 *
* www.olimex.com/dev/lpc-e2468.html *
**********************************************
..
U-Boot 1.3.1 (Apr 15 2008 - 16:32:08)
CPU: LPC2468 (ARM7tdmi-s from NXP)
running at 57.6 MHz (12 MHz crystal)
DRAM: 16 MB
Flash: 500 kB
NAND: No NAND device found!!!
0 MiB
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Hit any key to stop autoboot: 0
no devices available
Board is powered by SparkFun P/N TOL-00298 (9VDC/650mA). Board did not detect NAND out of the box, board did not boot Linux out of the box.
I have loaded U-Boot supply by Olimex with Flash Magic. U-Boot still report “No NAND device found!!!”. Flash IC is HY27UF081G2M.
**********************************************
* LPC-E2468 *
* www.olimex.com/dev/lpc-e2468.html *
**********************************************
..
U-Boot 1.3.1 (Oct 8 2008 - 04:07:55)
CPU: LPC2468 (ARM7tdmi-s from NXP)
running at 57.6 MHz (12 MHz crystal)
DRAM: 16 MB
Flash: 500 kB
NAND: No NAND device found!!!
0 MiB
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Hit any key to stop autoboot: 0
no devices available
no devices available
## Starting application at 0xA0008000 ...
lpc-e2468 # nand info
lpc-e2468 # nand erase
no devices available
lpc-e2468 #
lpc-e2468 # tftpboot 0xa0008000 vmlinux.bin
TFTP from server 192.168.2.145; our IP address is 192.168.2.162
Filename 'vmlinux.bin'.
Load address: 0xa0008000
Loading: #################################################################
#################################################################
###################
done
Bytes transferred = 2186536 (215d28 hex)
lpc-e2468 # nand write 0xa0008000 0x0 0x220000
no devices available
I have loaded U-Boot supply by Olimex with Flash Magic. U-Boot still report “No NAND device found!!!”. Flash IC is HY27UF081G2M.
It seems to me that Olimex E2468 schematic has a jumper to switch NAND chip select signal among two different control lines. Is the jumper correctly suited for your case?