I DIY a USB2JTAG board using a FT2232L, and I can halt, resume, and reset the Vivi on NOR flash in the S3C2440 Devboard using the USB2JTAG, so I think the hardware is OK.
Now I want to use it to debug some program to learn about ARM. I have tow questions, please give me some help.
The first is about the configuration file for OpenOCD, here is my config file
#daemon configuration
telnet_port 4444
gdb_port 3333
#debug_level 3
jtag_speed 1
#interface
interface ft2232
ft2232_device_desc "Dual RS232 A"
ft2232_layout "usbjtag"
ft2232_vid_pid 0x0403 0xcff8 #not used under Windows
jtag_speed 0
#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config trst_and_srst combined
#jtag_nsrst_delay 500
#jtag_ntrst_delay 500
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
#jtag_device 4 0x1 0xf 0x0032409d
jtag_device 4 0x1 0xf 0xe
#target configuration
daemon_startup reset_and_halt
#target <type> <endianess> <reset mode>
target arm9tdmi little reset_halt 0 arm920t
working_area 0 0x30000000 0x4000000 nobackup
run_and_halt_time 0 10
#flash configuration
#flash bank <driver> <base> <size> <chip_width> <bus_width> [driver_options ...]
flash bank cfi 0x00000000 0x200000 1 2 0
The S3C2440 has 64MB SDRAM (0x3000000-0x340000000, selected by nGCS6),
and 2M NOR Flash (0x00000000-0x00200000, selected by nGCS0),
it also have 64MB NAND flash
Does the above OpenOCD configuration right ?
The second is about the ldscript.
I modify the ldscript for AT91SAM7 come with the winarm toolchain, the only thing I changed is the MEMORY section
MEMORY
{
CODE (rx) : ORIGIN = 0x30000000, LENGTH = 0x00003000
DATA (rw) : ORIGIN = 0x30003000, LENGTH = 0x00001000
STACK (rw) : ORIGIN = 0x30004000,LENGTH = 0x00000000
}
/* Section Definitions */
SECTIONS
{
/* first section is .text which is used for code */
. = 0x0000000;
.text : { *cstartup.o (.text) }>CODE =0
.text :
{
*(.text) /* remaining code */
*(.glue_7t) *(.glue_7)
} >CODE =0
. = ALIGN(4);
/* .rodata section which is used for read-only data (constants) */
.rodata :
{
*(.rodata)
} >CODE
. = ALIGN(4);
_etext = . ;
PROVIDE (etext = .);
/* .data section which is used for initialized data */
.data : AT (_etext)
{
_data = . ;
*(.data)
SORT(CONSTRUCTORS)
} >DATA
. = ALIGN(4);
_edata = . ;
PROVIDE (edata = .);
/* .bss section which is used for uninitialized data */
.bss :
{
__bss_start = . ;
__bss_start__ = . ;
*(.bss)
*(COMMON)
}
. = ALIGN(4);
__bss_end__ = . ;
__bss_end__ = . ;
_end = .;
. = ALIGN(4);
.int_data :
{
*(.internal_ram_top)
}> STACK
PROVIDE (end = .);
/* Stabs debugging sections. */
.stab 0 : { *(.stab) }
.stabstr 0 : { *(.stabstr) }
.stab.excl 0 : { *(.stab.excl) }
.stab.exclstr 0 : { *(.stab.exclstr) }
.stab.index 0 : { *(.stab.index) }
.stab.indexstr 0 : { *(.stab.indexstr) }
.comment 0 : { *(.comment) }
/* DWARF debug sections.
Symbols in the DWARF debugging sections are relative to the beginning
of the section so we begin them at 0. */
/* DWARF 1 */
.debug 0 : { *(.debug) }
.line 0 : { *(.line) }
/* GNU DWARF 1 extensions */
.debug_srcinfo 0 : { *(.debug_srcinfo) }
.debug_sfnames 0 : { *(.debug_sfnames) }
/* DWARF 1.1 and DWARF 2 */
.debug_aranges 0 : { *(.debug_aranges) }
.debug_pubnames 0 : { *(.debug_pubnames) }
/* DWARF 2 */
.debug_info 0 : { *(.debug_info .gnu.linkonce.wi.*) }
.debug_abbrev 0 : { *(.debug_abbrev) }
.debug_line 0 : { *(.debug_line) }
.debug_frame 0 : { *(.debug_frame) }
.debug_str 0 : { *(.debug_str) }
.debug_loc 0 : { *(.debug_loc) }
.debug_macinfo 0 : { *(.debug_macinfo) }
/* SGI/MIPS DWARF 2 extensions */
.debug_weaknames 0 : { *(.debug_weaknames) }
.debug_funcnames 0 : { *(.debug_funcnames) }
.debug_typenames 0 : { *(.debug_typenames) }
.debug_varnames 0 : { *(.debug_varnames) }
}
Everytime I download the code from arm-elf-insight to Openocd, it says “download failed”.
I have searched the forum, didn’t find some similiar use case. Is there some sample source code for S3C2440 using gnutool chian and can be debugged with OpenOCD ?
Any help is appreciated ![]()