I recently attempted to repair a laptop that had a daughterboard connector broken off, but in the process, I let the iron get too hot and melted the plastic on the connector. Can anybody help me identify this part so I can find a replacement? It has 24 pins, pitch is 0.5mm or less, I haven’t been able to accurately measure it.
(Click for a larger photo)
And here’s the mating connector (which is fine)
[
](Imgur: The magic of the Internet)](Imgur: The magic of the Internet)