Hi all, first post and thread here.
I’m working on a project to give bluetooth capability to my ZuneHD. I bought and received the purpletooth jamboree board and a LiPo battery. I got the board to hook up to my G-pop bluetooth speaker once, then i turned it off to go buy a male to male audio cble to connect the board to my ZuneHD. After i turned it on again all i get is a blue blinking LED (1 i think) and nothing connects. I read in the hookup guide something about the chip not being able to reconnect if anything changes in the connection stored on the board.
This is my first project and really my first time working with a custom build electronic. Any sugestions on how to get the board to work with bluetooth connections?
Do i need to include a micro controller with the board like an aruino, or can i access it via the micro usb port build in to program and configure it to work? Thanks for aany help anyone can give ![]()