Need help - XBee and U.FL

Hey everyone!

It’s my first time working with an XBee, and I’ve hit a small hitch. (It’s dumb.)

I cannot get my antennae to mate with my XBees. They’re U.FL. I’m using [these XBees (not the series 2.5 in the picture, the newer series 2) and [these antennae.

No matter how centered I get the connector, the antenna’s connector will not mate with the XBee. I’m pressing more than hard enough. Heck, I’ve even worked with U.FL before (in my sister’s laptop) and it was nothing like this - the connectors just popped right on.

I have two XBees and multiple antennae, and none of the antennae will attach to either of the XBees. I even RMA’d the antennae because the connectors looked a bit bent (both the ones I had used as well as some that were unopened). Nothing seems to work.

[I took a (blurry) picture, if that helps at all.

Thanks everyone!](ImageShack - Best place for all of your image hosting and image sharing needs)](A24-HABUF-P5I Digi | Mouser)](XBee 2mW U.FL Connection - Series 2 (ZigBee Mesh) - WRL-10417 - SparkFun Electronics)