I am trying to connect the SAM9-L9260 development board to the computer. I am using the Keil uVison3 as a compiler, but when I try to load the code the compiler gives me error saying “ULINK - ARM Error: No ULINK device found”. It seems that the problem is there because of the missing driver. In the windows device manager I am missing driver for RNDIS/Ethernet Gadget which is used for SAM9-L9260 board. I can’t find this driver on the CD that came with the board. Could anyone please help me find this driver? Thanks,
- Himanshu