the site there has test code that i’ve been trying to get running in avr studio 4. i haven’t been able to compile it, having not been able to find the and include “mega128.h” and “delay.h”
would be great if i could get some code to start working.
have spent many hours trying to find somewhere to start but haven’t had any luck.
natew021:
having not been able to find the and include “mega128.h” and “delay.h”
Are you using avr-gcc (WINAVR)? If so, I assume you've installed WINAVR. Instead of including "mega128.h", use:```
#include
```
The compiler will include the correct header file based on yu device setting.
Also, for “delay.h”, you want:``` #include <avr/delay.h>
have you read the newbie stuff on WinAVR that is on avrfreaks.net?
You might also want the simplicity of a low cost IDE for GCC on the AVR - such as Atmanecl.net. It’s pretty good and makes the compiler learning curve much easier - no make files, and an ordinary IDE experience. There’s a demo trial.
fgcity:
Why would i want a low cost IDE for GCC on AVR when the AVR studio is free and comes with the GCC compiler?
well, I like the IDE because it greatly simplifies creating and sustaining a project. Apparently a lot of others do too, as there are several free and inexpensive IDEs for GCC - project files + editor + flash programmer in one UI. I guess I’m accustomed to an IDE having used such for all languages for several years.
Some folks are OK with independent programs. And AVRStudio with GCC isn’t an IDE in my opinion.