Needing help with load cell/arduino/esp32/Embedded C code alterations; willing to pay/donate

Hi there ! none of the optional tags mean anything to me, sorry, Arduino and ESP32 are super exciting to me but I really am a very beginner at this stuff. I am looking for someone who can meet with me on zoom and help me one step at a time get my project working. I would love to get help from one person if at all possible. I have successfully installed arduino software, uploaded sketches and connected circuit boards to the Arduino controlling LED lights with transistors so I can do very basic stuff but nothing complex. I have a Load Cell and a set of strain gauges that I want to connect firstly to an Arduino then after things are working I want to connect these sensors to an ESP32 and I want help altering the Embedded C code so that the Firmware will direct event driven decisions depending on the input from the Force sensors. The sensors will be in motion (physically being moved up and down) so there will have to be a comparitor circuit looking at what the weight of the object would be at rest and what it should be while following this motion. Please contact me.
Thank you for reading !
: )