New Ethernet shield SPI problem

Hello guys,

I have the new ethernet shield with sd slot integrated. It is supposed that to be able to work with the SD I should disable the ethernet SPI by putting pin 10 output high. So I assume that to connect another SPI device I can do the same, isn’t it ? But it doesn’t work

It is supposed that in the new versions of the Ethernet shields (like mine) the W5100 SPI bug has been solved (I think I can see this in the schematic because because there an inverter to the SPI “SS” and the output of the inverter is connected to the “SEN” pin on the '5100) Am I correct?

I have a problem to connect another shield through SPI if I mount it over the ethernet althoght I set pin 10 and 4 output and high.

Any help would be higly appreciated