New OpenOCD Version from Yagarto

Hello I do not know whats wrong but the new OpenOCD + Yagarto dosen’t work.

Open On-Chip Debugger (2008-06-19 19:00) svn: 717

URL: http://svn.berlios.de/svnroot/repos/openocd/trunk

Info: options.c:50 configuration_output_handler(): jtag_khz: 10, 1500

Info: options.c:50 configuration_output_handler(): Open On-Chip Debugger (2008-06-19 19:00) svn: 717

Info: jtag.c:1389 jtag_examine_chain(): JTAG device found: 0x4f1f0f0f (Manufacturer: 0x787, Part: 0xf1f0, Version: 0x4)

Info: jtag.c:1389 jtag_examine_chain(): JTAG device found: 0x4f1f0f0f (Manufacturer: 0x787, Part: 0xf1f0, Version: 0x4)

Info: target.c:237 target_init_handler(): executing reset script ‘F:\Programmieren\ARM\Yagarto\test\prj\lpc2148_reset.script’

looks okay.

But when i start the debugger:

target remote localhost:3333

0x7fffd2c2 in ?? ()

monitor reset

monitor sleep 500

monitor poll

monitor soft_reset_halt

monitor arm7_9 sw_bkpts enable

monitor mww 0xE01FC040 0x0002

monitor mdw 0xE01FC040

needed for gdb 6.8 and higher

Undefined command: “”. Try “help”.

set mem inaccessible-by-default off

load main.elf

main.elf: No such file or directory.

break main

No symbol table is loaded. Use the “file” command.

continue

Pleas has anybody new setup files.

The new Sample for lpc2148 from Yagarto doesn’t work i think.

thanks mgiaco

Try to remove the comment "# needed for gdb 6.8 and higher "

thanks i will try it, now i am not at home.

ysagon: No it doesn’t work. I do not understand what’s wrong. I use the sample lpc2148 from Yagarto.

Open On-Chip Debugger (2008-06-19 19:00) svn: 717

URL: http://svn.berlios.de/svnroot/repos/openocd/trunk

Info: options.c:50 configuration_output_handler(): jtag_khz: 10, 1500

Info: options.c:50 configuration_output_handler(): Open On-Chip Debugger (2008-06-19 19:00) svn: 717

Info: jtag.c:1389 jtag_examine_chain(): JTAG device found: 0x4f1f0f0f (Manufacturer: 0x787, Part: 0xf1f0, Version: 0x4)

Info: jtag.c:1389 jtag_examine_chain(): JTAG device found: 0x4f1f0f0f (Manufacturer: 0x787, Part: 0xf1f0, Version: 0x4)

Info: target.c:237 target_init_handler(): executing reset script ‘F:\Programmieren\ARM\Yagarto\test\prj\lpc2148_reset.script’

target remote localhost:3333

0x7fffd2c8 in ?? ()

monitor reset

monitor sleep 500

monitor poll

monitor soft_reset_halt

monitor arm7_9 sw_bkpts enable

monitor mww 0xE01FC040 0x0002

monitor mdw 0xE01FC040

needed for gdb 6.8 and higher

Undefined command: “”. Try “help”.

set mem inaccessible-by-default off

Undefined command: “”. Try “help”.

load

No executable file specified.

Use the “file” or “exec-file” command.

break main

No symbol table is loaded. Use the “file” command.

continue

Everything works fine no. It was a problem with Zylin.

Thanks mgiaco