NO COM PORT FOR STM32 THING PLUS

I’ve seen this post previously, but no replies. Not sure if anyone figured out what is going on?

I followed the basic steps to load the blinky program.

If I follow these steps and press the upload button in the Arduino IDE 2.2.1, the program loads. When I unplug and re-plug the STM32 board with the USB cable, the program runs.

However, I cannot open a putty session to view the “Hello World!” message.

Looking at device manager only two COM ports are listed COM1 and COM3. Neither of these COM ports connect to the STM32.

Can anyone let me know why this super basic setup procedure on the Sparkfun website does not work? Any solution to make it work?

Thanks

Does the Hello, World show when running the Arduino Serial Monitor?

Same issue here. I have a Sparkfun STM32 Things Plus. I am using VS Code and arduino-cli. The board showed up as COM6 before my first upload. After the first upload, I have no COM6 – I can still upload to that port however. I’m using the defaults for all the USB/Serial board configuration settings. The COM6 port is missing, so neither the “arduino-cli monitor” command nor the VS Code Serial Monitor function can connect.

I have tried this with both the 2.0.0 and 2.1.0 releases of the Sparkfun STM32 board. Same outcome.

I am having a similar issue with a brand new STM32 Micromod. I can upload but the program wont run and the serial port is always missing. A bit of swapping with spare boards and spare datalogging carriers indicates the issue is a faulty STM32 processor board. So yours may well be a faulty Thing Plus.
Lockie

https://community.sparkfun.com/t/stm32-thing-plus-no-show-in-com-ports-but-does-show-boot-loader/44524

I am having a similar issue with a brand new Sparkfun STM32 Thing plus. No COM port has ever appeared when you plug it in or put it in boot mode. I tried reflashing through the STMCubeProgrammer. It can see the device over USB, but can not connect via ST-Link.

Are there any new suggestions for how to fix this? Do I have a bad board since it came like this out of the box? Thank you in advance for any advice you can provide!

Did you end up finding a solution to this?