Nordic Serial Interface Board compatible with nRF24L01+ ?

Is the Nordic Serial Interface Board module compatible with the nRF24L01+ Transceiver modules?

The Serial Board spec says it works with the nRF24L01, nRF2401A, and RF-24G but I’m hoping it also works with the nRF24L01+.

If it’s not compatible how difficult would it be to modify the software on the serial board so that it is compatible?

  • Chris Graham

Hi Chris,

From what I can tell, the serial board will work fine with the nRF24L01+, but treats it as a backward-compatible nRF2401A, and so won’t use the advanced features of the +. The firmware for the serial board is available though, and at least one user has modified it to run faster and use the newer features of the +. See the comments on the product page for information.

Awesome website and projects by the way! 8)