NOT SAVED FILE IN GM862 PYTHON

I HAVE TROUBLES WHEN I TRY TO COMMUNICATE WITH GM862, ONLY

WITH 115200,8,N,1,HARDWARE FLOW CONTROL.

I AM USING HYPERTERMINAL, IF I WORK WHITHOUT HARDWARE FLOW

CONTROL , I CAN CONNECT WITH GM862.

PLEASE, IF SOME ONE CAN HELP ME .

the solution was to configure hyperterminal 115200,8,n,1 without hardware flow control, and it is the same to send AT commands,and

DTR needs to set low( 0 volts)