leon_heller:
The OP is using the nRF2401, not the nRF24L01. Brennen’s stuff won’t be much use to him.
Indeed. One of these days I’m gonna break out my 2401’s and put them through their paces, but I haven’t gotten around to it just yet. Especially considering that the 24L01 will beat the pants off of the 2401 in pretty much every category. :twisted:
I have a couple of the original MiRFs with the nRF2401A but there isn’t much point in using them now, the nRF24L01 is much better. The range is quite good with the little 1/4 wave antenna - much better than the MiRF V2 with the ceramic antenna.
leon_heller:
The range is quite good with the little 1/4 wave antenna - much better than the MiRF V2 with the ceramic antenna.
I definitely agree. The range is terrible with the ceramic guy. I even retro-fitted one of my units that had the ceramic antenna to the duck antenna that Sparkfun sells and the range is much better.
Even at full power, I was getting quite a few errors at 10 feet when there was a significant source of RF in the 2.4 GHz range around (wireless router). I never tested the range too much more than that, or once I put on the duck antenna.