Nu-Link debugger driver for IAR 6.21

Nuvoton updated the Nu-Link debugger (rev1.17.5218) for latest IAR 6.21,

which supports to debug their cortex M0 chips, such as M051 and NUC100 series.

Please download this version if you’re interested in it.

http://www.nuvoton-m0.com/forum.php?mod … a=page%3D1

Features of the newest Nu-Link debugger,

  1. Supports to debug Cortex M0 chips in Keil or IAR environment.

  2. Supports flash breakpoints, so that the maximum number of breakpoints is unlimited.

  3. The Nu-Link debugger is also a writer.

It can be used as offline programmer to write M0’s flash without a PC.

  1. Protection for customers code when offline programming

a. Can set the maximum writing count

b. Encrypt data saved in Nu-Link debugger

c. Encrypt data transferred between Nu-Link debugger and target M0 chips when programming.