Hi, I’m working on a project that I’m about 80% of the way finished with. I’m replacing my stock radio with a custom built setup that will play music, control my exhaust system (more on that*), and display some live stats. The car is a 2007 Z06 Corvette. It’s running on a pi3b+ with a 7" touchscreen and the QWIIC quad relay to control the Bose factory amplifier** and exhaust. The GUI is 90% finished with the audio and exhaust control portion 100% operational and stats that I’d like to see statically coded. I’m trying to work with the OBDII board and I’m not quite sure if I should have bought the regular CAN shield instead. The site below says that my car uses CAN 500kbps 11bit. Does it sound like I can get the TPMS sensor information from the car? Does the board support the lower speed SWCAN protocol if I need to poke around there instead? I’d also try to get my steering wheel controls to work for the radio. I can share more information if anyone is interested.
https://pinoutguide.com/CarElectronics/ … nout.shtml
*It comes with the dual-mode exhaust that has valves that open and close depending on the speed of the engine and throttle position. Right now I have the fuse removed on the system so that the valves are always opened
**The amplifier is turned on and off the same way an aftermarket one would be, through a 12v signal from a head unit. When the pi powers up and turns on the sound, it makes a popping noise through the speaker output. I use the relay to keep the amp off until after the sound driver/service is loaded.