I have an older motor home (1992) with a rather sophisticated alarm system. The original system would monitor the door, the hood, all of the cargo doors, two sensors for glass breakage, movement, smoke alarm, remote sensor in the towed vehicle, and it would page you if the alarm was activated. Each door has a wireless transmitter on it and each smoke sensor also. Since the company that made it is out of business and I can’t find anyone that has any information on it so I purchased a newer alarm which sounds like it can fill the bill except for the fact that I don’t have any way of receiving the signals from each door etc. Is there someway of finding out what the transmitters are sending out so I can connect them to a receiver which would fire a switch for the new alarm?