OLED control via SPI from AVR

On more update.

I am really surprised that there were no other replies to this at all. Is no one else using this board?

Anyway. It seems as if the new version of this board is not compatible with the old version. The display driver chip on the old board was an SSD1339 and the new one is an SSD1351. These boards seem identical in pin-out but are not %100 command compatible. There does not appear to be any kind of Draw commands or clear window command. Also the documentation that you can currently find on the net about it is a bit flawed (referring to the pdf datasheet from the manufacturer themselves). I believe it is a very early version of the document. I have requested a new datasheet but have not received a response yet.

It should be known that the link to thdatasheet for the new Sparkfun OLED carrier board is actually the datasheet for the old carrier board and that datasheet still has a link to the old SSD1339 datasheet.

I have contacted Sparkfun tech support about it and did my best to explain the issue but I have not heard a response back from them.