Hi Phalanx … can you tell me if the Olimex ARM-USB-OCD JTAG programmer is compatible - ie with no hassle - with the NXP/RED LPCXpresso IDE ? Im starting an LPC1343 USB project …
Thks heaps - its just that the Australian distributor Dontronics has the Olimex stuff in stock…
Rgds
DonW
             
            
              
              
              
            
            
           
          
            
            
              Hi deadsherrif,
ARM is not really my area of expertise so I won’t be of much help. I also don’t work for Sparkfun so I can’t just run over and ask someone.
I’m sure someone else on this forum will chime in though.
Sorry and good luck!
-Bill
             
            
              
              
              
            
            
           
          
            
            
              The Code Red IDE for the LPCXpressso will only work with the interface on that board. The standard version might work with the ARM-USB-OCD JTAG.
             
            
              
              
              
            
            
           
          
            
            
              
leon_heller:
The Code Red IDE for the LPCXpressso will only work with the interface on that board. The standard version might work with the ARM-USB-OCD JTAG.
Thks Leon … had to ask …and someoine else corrected my other error - that JTag is not SWDebug used on the LPC1000’s either …silly me
             
            
              
              
              
            
            
           
          
            
            
              
leon_heller:
The Code Red IDE for the LPCXpressso will only work with the interface on that board. The standard version might work with the ARM-USB-OCD JTAG.
Also Leon …if it is said that safeRTOS or FreeRTOS is , say, 4.5KB in size, is this “thumbed” for the 32 bit-ers memory word size ?
It seems time we all rearranged the brain and talked in “words” …now 32 bit devcies are as cheap as 8 bit ones …
Rgds
DonW