Starting kernel …
Uncompressing Linux… … done, booting the kernel.
Linux version 2.6.23 (ivan@debian.l123.org) (gcc version 4.1.2) #5 PREEMPT Sun O ct 14 02:01:51 EEST 2007
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: Olimex SAM9-L9260
Memory policy: ECC disabled, Data cache writeback
Clocks: CPU 198 MHz, master 99 MHz, main 18.432 MHz
CPU0: D VIVT write-back cache
CPU0: I cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists in Zone order. Total pages: 16256
Kernel command line: mem=64M console=ttyS0,115200, noinitrd=linux root=/dev/mtdb lock1 rootfstype=jffs2
AT91: 96 gpio irqs in 3 banks
PID hash table entries: 256 (order: 8, 1024 bytes)
Console: colour dummy device 80x30
console [ttyS0] enabled
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 64MB = 64MB total
Memory: 61336KB available (2732K code, 686K data, 108K init)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
Generic PHY: Registered new driver
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
NetWinder Floating Point Emulator V0.97 (double precision)
audit: initializing netlink socket (disabled)
audit(0.570:1): initialized
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
io scheduler noop registered
io scheduler anticipatory registered
io scheduler deadline registered
io scheduler cfq registered (default)
atmel_usart.0: ttyS0 at MMIO 0xfefff200 (irq = 1) is a ATMEL_SERIAL
atmel_usart.1: ttyS1 at MMIO 0xfffb0000 (irq = 6) is a ATMEL_SERIAL
atmel_usart.2: ttyS2 at MMIO 0xfffb4000 (irq = 7) is a ATMEL_SERIAL
RAMDISK driver initialized: 16 RAM disks of 8192K size 1024 blocksize
loop: module loaded
MACB_mii_bus: probed
eth0: Atmel MACB at 0xfffc4000 irq 21 (3e:36:65:ba:6f:be)
eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
block2mtd: version $Revision: 1.30 $
NAND device: Manufacturer ID: 0xec, Chip ID: 0xdc (Samsung NAND 512MiB 3,3V 8-bi t)
Scanning device for bad blocks
Bad eraseblock 0 at 0x00000000
Bad eraseblock 1 at 0x00020000
Bad eraseblock 2 at 0x00040000
Bad eraseblock 3 at 0x00060000
Bad eraseblock 8 at 0x00100000
Bad eraseblock 9 at 0x00120000
Bad eraseblock 10 at 0x00140000
Bad eraseblock 11 at 0x00160000
Bad eraseblock 12 at 0x00180000
Bad eraseblock 13 at 0x001a0000
Bad eraseblock 14 at 0x001c0000
Bad eraseblock 15 at 0x001e0000
Bad eraseblock 16 at 0x00200000
Bad eraseblock 17 at 0x00220000
Bad eraseblock 18 at 0x00240000
Bad eraseblock 19 at 0x00260000
Bad eraseblock 20 at 0x00280000
Bad eraseblock 21 at 0x002a0000
Bad eraseblock 32 at 0x00400000
Bad eraseblock 33 at 0x00420000
Bad eraseblock 34 at 0x00440000
Bad eraseblock 35 at 0x00460000
Bad eraseblock 36 at 0x00480000
Bad eraseblock 37 at 0x004a0000
Bad eraseblock 38 at 0x004c0000
Bad eraseblock 39 at 0x004e0000
Bad eraseblock 40 at 0x00500000
Bad eraseblock 41 at 0x00520000
Bad eraseblock 42 at 0x00540000
Bad eraseblock 43 at 0x00560000
Bad eraseblock 44 at 0x00580000
Bad eraseblock 45 at 0x005a0000
Bad eraseblock 46 at 0x005c0000
Bad eraseblock 47 at 0x005e0000
Bad eraseblock 48 at 0x00600000
Bad eraseblock 49 at 0x00620000
Bad eraseblock 50 at 0x00640000
Bad eraseblock 51 at 0x00660000
Bad eraseblock 52 at 0x00680000
Bad eraseblock 53 at 0x006a0000
Bad eraseblock 54 at 0x006c0000
Bad eraseblock 55 at 0x006e0000
Bad eraseblock 56 at 0x00700000
Bad eraseblock 57 at 0x00720000
Bad eraseblock 58 at 0x00740000
Bad eraseblock 59 at 0x00760000
Bad eraseblock 60 at 0x00780000
Bad eraseblock 61 at 0x007a0000
Bad eraseblock 62 at 0x007c0000
Bad eraseblock 63 at 0x007e0000
Bad eraseblock 976 at 0x07a00000
Bad eraseblock 2060 at 0x10180000
Bad eraseblock 2283 at 0x11d60000
Creating 2 MTD partitions on “NAND 512MiB 3,3V 8-bit”:
0x00000000-0x00a00000 : “Bootloader Area”
0x00a00000-0x20000000 : “User Area”
at91_ohci at91_ohci: AT91 OHCI
at91_ohci at91_ohci: new USB bus registered, assigned bus number 1
at91_ohci at91_ohci: irq 20, io mem 0x00500000
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 2 ports detected
Initializing USB Mass Storage driver…
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver libusual
udc: at91_udc version 3 May 2006
ether gadget: using random self ethernet address
ether gadget: using random host ethernet address
usb0: Ethernet Gadget, version: May Day 2005
usb0: using at91_udc, OUT ep2 IN ep1 STATUS ep4
usb0: MAC 46:0c:47:7d:59:ca
usb0: HOST MAC 82:63:1e:fe:34:b5
usb0: RNDIS ready
mice: PS/2 mouse device common for all mice
TCP cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 1
NET: Registered protocol family 17
NET: Registered protocol family 15
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
VFS: Mounted root (jffs2 filesystem).
Freeing init memory: 108K
Warning: unable to open an initial console.
Kernel panic - not syncing: No init found. Try passing init= option to kernel.
and then freeze in this screen but Stat Led is Blinking .
Anyone can help me fix this problem