I recently bought one of the Olimex USB JTAG devices. I plugged it in, it showed up as COM2 using the latest FTDI drivers.
I started up AVR Studio 4.01 with the services pack 3, I beleive.
It asked to upgrade the firmware, I pressed the “OK” button or whatever it was. An application popped up to do the upgrade.
I pressed the “Program” button. It went through three bars of the Erase stage and stopped. After a while it gave me an error, which I didn’t note down.
After that AVR Studio does not find the device.
Any suggestions?
Update: Got a second one from Spark fun, did exactly the same thing… Now I have two dead programmers. Anybody? Any ideas at all?
Here is the question: can I force AVRProg to reflash the device?
Is there any other software that can do it properly?
Or I just wasted my money on buying olimex product?
BTW USB->COM is set to COM2 now. So I technically should not get anymore issues.
Olimex should supply a warning about these issues in first place, as their products are obviously targeted for beginers, or atleast provide a tool to recover from that flaw.