This is an old thread but I’m adding to it because the original poster is right, and it does work, but I never fully solved the ideal context.
First, the motors must be efficient. I had two that were, once, in times when I needed to sell them to get money. Foolish, I can’t trace them now to replicate what I did!
I know they were about 60mm wide and 60mm long (not including shaft length), round, with square flanges, a hybrid type with 200 steps and 6 wires. Probably bipolar. Many motors won’t work, and to do so usefully they must overcome losses and both motors should ideally be the same type and be designed for 24V or more, though a large one driving a small one might work well, but it would take someone with a LOT of motors and spare time to find out!
A wide diameter seems to help, as does a large step count for lower turn speed to get strong pulses. A stepper motor can drive STRONG pulses, enough to give electric shocks if driven manually at high speed with a strong twist on the drive shaft. Some people have suggested motors for direct drive by wind power, and motors that work well for that may also be good for direct-coupled drive.
An example of why this is so useful: turning a magnetic loop antenna. It is vital to eliminate RFI/EMI, so drive circuitry that can emulate the clean sinusoidal output of a ‘backdriven’ motor is expensive and complex. Given that listening to the receiver output is the best way to gauge antenna orientation for peaking and nulling, it does not matter if the hand-driven motor results in slipped sync at times, so an entirely passive system can solve the RFI problem, and the saving in time and money, and the robustness of the method, make it entirely worth doing. Holding torque is good in any system where this effect is set up well, and if an antenna were swung by the wind, the user could immediately tell by movement in the motor at their end, with no need for electronic feedback! Adjusting user technique to best effect would be a lot easier than getting good tone from a violin bow, if the motors were chosen correctly.
For a wide loop antenna a simple belt gear could overcome losses and also give fine adjustment of nulls, and also allow the external motor to be shrouded to protect it from bad weather..
There may be many applications but that example is a really good one, so if anyone has practical advice to narrow down the selection criteria for such use of stepper motors, please post, because it’s a good thing to explore.. A low-maintenance, easily built system like this might easily outlive the person who uses it, so as a saving in waste parts it is excellent. Stepper motors able to do this might cost more than those that can’t., but the difference in price might be a lot smaller than the cost of active electronics.