Ful error message=
Arduino: 1.8.13 (Windows 10), Board: “Arduino Leonardo”
Warning: Board arduino:avr:atmega16-8 doesn’t define a ‘build.board’ preference. Auto-set to: AVR_ATMEGA16-8
Sketch uses 23124 bytes (80%) of program storage space. Maximum is 28672 bytes.
Global variables use 490 bytes (19%) of dynamic memory, leaving 2070 bytes for local variables. Maximum is 2560 bytes.
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, COM10, } => {COM10, }
Found upload port: COM10
D:\Program Files (x86)\arduino ide\arduino-1.8.13\hardware\tools\avr/bin/avrdude -CD:\Program Files (x86)\arduino ide\arduino-1.8.13\hardware\tools\avr/etc/avrdude.conf -v -patmega32u4 -cavr109 -PCOM10 -b57600 -D -Uflash:w:C:\Users\Stef_\AppData\Local\Temp\arduino_build_874292/ssd1306_128x32_i2c.ino.hex:i
avrdude: Version 6.3-20190619
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is “D:\Program Files (x86)\arduino ide\arduino-1.8.13\hardware\tools\avr/etc/avrdude.conf”
Using Port : COM10
Using Programmer : avr109
Overriding Baud Rate : 57600
AVR Part : ATmega32U4
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PA0
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
eeprom 65 20 4 0 no 1024 4 0 9000 9000 0x00 0x00
flash 65 6 128 0 yes 32768 128 256 4500 4500 0x00 0x00
lfuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
efuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
lock 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
Programmer Type : butterfly
Description : Atmel AppNote AVR109 Boot Loader
Connecting to programmer: .
Found programmer: Id = “CATERIN”; type = S
Software Version = 1.0; No Hardware Version given.
Programmer supports auto addr increment.
Programmer supports buffered memory access with buffersize=128 bytes.
Programmer supports the following devices:
Device code: 0x44
avrdude: devcode selected: 0x44
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.00s
avrdude: Device signature = 0x1e9587 (probably m32u4)
avrdude: reading input file “C:\Users\Stef_\AppData\Local\Temp\arduino_build_874292/ssd1306_128x32_i2c.ino.hex”
avrdude: writing flash (23124 bytes):
Writing | ################################################## | 100% 2.17s
avrdude: 23124 bytes of flash written
avrdude: verifying flash memory against C:\Users\Stef_\AppData\Local\Temp\arduino_build_874292/ssd1306_128x32_i2c.ino.hex:
avrdude: load data flash data from input file C:\Users\Stef_\AppData\Local\Temp\arduino_build_874292/ssd1306_128x32_i2c.ino.hex:
avrdude: input file C:\Users\Stef_\AppData\Local\Temp\arduino_build_874292/ssd1306_128x32_i2c.ino.hex contains 23124 bytes
avrdude: reading on-chip flash data:
Reading | #############################################An error occurred while uploading the sketch
| 100% 0.80s
avrdude: verifying …
avrdude: verification error, first mismatch at byte 0x2480
0xff != 0x2a
avrdude: verification error; content mismatch
avrdude done. Thank you.
This report would have more information with
“Show verbose output during compilation”
option enabled in File → Preferences.