Hello,
I’m having issues with my Microview. I’ve uploaded a program and it works perfect…but when I edit the code just slightly then I get the following errors:
Arduino: 1.8.12 (Mac OS X), Board: “Arduino Uno”
Sketch uses 14804 bytes (45%) of program storage space. Maximum is 32256 bytes.
Global variables use 1371 bytes (66%) of dynamic memory, leaving 677 bytes for local variables. Maximum is 2048 bytes.
avrdude: verification error, first mismatch at byte 0x30d8
0x4a != 0x4e
avrdude: verification error; content mismatch
avrdude: verification error; content mismatch
**As a note I changed a temperature setting (hightemp = 125 to hightemp=127, and lowtemp=59 to lowtemp =61) and the program will compile fine but won’t upload now. However if I change the code back to the original it uploads just fine.