Hi there. I’m super new at this and am having some troubles. I’m trying to use a serial terminal to log into an Openlog Artemis and it won’t show up at all. (On the tty level) so I can’t log into it.
I’ve tried two different openlogs on multiple computers with no success. Just to rule out my cable and the fact that I’m doing something wrong I tried a pro micro and it shows right up. Any thoughts?
Yes I do and it does log data. Honestly I could deal with most of the default settings except I want to lower my sample speed for a long duration data logging project. B
It’s been a bit since I’ve had a chance to get back to this… I have checked the port setting and those are correct and the terminal program doesn’t even find the open log. Naltieri is on the right track as the boards don’t seem to be found by the Device manager(or equivalent). I Have been using computers that should have the appropriate drivers installed and have tried installing them just in case they weren’t there for some reason.
Ensure you have admin rights on the PC you use, if the CH 340 driver has installed correctly you will see in the Windows device manager under ports when you plug the Open log Artemis into a USB port and it will be assigned a Com port number. Check that you havent got two instances of your terminal program or other serial program running and all trying to use same Com port number. You might have to press the reset button on the board, also try a different USB type C cable.