Hello friends,
I am working on a project that largely revolves around the ESP32 WROVER. The device is going to be at a remote location for testing, but I’ll need to be able to get the serial output.
I think that the OpenLog might be a good solution here, but I’m not 100% positive. I’ve been reading this, and have come away with more questions: https://learn.sparkfun.com/tutorials/op … okup-guide
My board has 4 pins broken out from the ESP32: rx, tx, vcc, gnd. Will those be sufficient to write to the OpenLog? Or do I need to figure out how to get a wire for dtr and blk (gnd?)
Do I need to somehow include the OpenLog library in my source for the ESP32 program? It is written using PlatformIO using C++, not Arduino. I am hoping that using a config.txt file I can just have it write all serial input it receives to a single file. Is that the case?
Thanks for any guidance here!