Hello. I faced the following problem. I need to read cyclicly a region of RAM of the STM32F217. Now I do it via dump_image command. I faced with the fact that no matter what I set the speed through adapter_khz, in fact, it remains the same. I checked it with J-Link v8 and ST-Link v.2 debuggers. The screenshots shown OpenOCD startup parameters and the actual speed, which was got via logic analyzer from the TCK (SWCLK) pin.
ST-Link v.2 950 kHz
ST-Link v.2 1800 kHz
ST-Link v.2 4000 kHz
J-Link v.8 8000 kHz
What I missed or doing wrong? Does someone make experements with speed of uploading/downloading data via OpenOCD?](http://itmages.ru/image/view/3110235/ec505241)](http://itmages.ru/image/view/3110233/91b4dd9f)](http://itmages.ru/image/view/3110229/3be55c3b)](http://itmages.ru/image/view/3110223/a427eee6)