tried openocd r1836 and r1938 with the same results.
I need to flash an AT91SAM7X256 (the board is evaluation board from atmel) with an Amontec jtagkey-tiny.
My PC runs ubuntu linux 8.10 64bit, and I use libftdi 0.16 (configured as defaults)
PC is an intel core2 q8300 and 4GB ram
I run openocd with the following command line
$ sudo openocd -f scrips/jtagkey.cfg -f scrips/sam7x256.cfg -d 3
with scrips, jtagkey.cfg:
#
# Amontec JTAGkey
#
# http://www.amontec.com/jtagkey.shtml
#
#daemon configuration
telnet_port 4444
gdb_port 3333
interface ft2232
ft2232_device_desc "Amontec JTAGkey A"
ft2232_layout jtagkey
ft2232_vid_pid 0x0403 0xcff8
and sam7x256.cfg
#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config srst_only srst_pulls_trst
if { [info exists CHIPNAME] } {
set _CHIPNAME $CHIPNAME
} else {
set _CHIPNAME sam7x256
}
if { [info exists ENDIAN] } {
set _ENDIAN $ENDIAN
} else {
set _ENDIAN little
}
if { [info exists CPUTAPID ] } {
set _CPUTAPID $CPUTAPID
} else {
set _CPUTAPID 0x3f0f0f0f
}
jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf
-expected-id $_CPUTAPID
set _TARGETNAME [format "%s.cpu" $_CHIPNAME]
target create $_TARGETNAME arm7tdmi -endian $_ENDIAN -chain-position
$_TARGETNAME -variant arm7tdmi
$_TARGETNAME configure -event reset-init {
# disable watchdog
mww 0xfffffd44 0x00008000
# enable user reset
mww 0xfffffd08 0xa5000001
# CKGR_MOR : enable the main oscillator
mww 0xfffffc20 0x00000601
sleep 10
# CKGR_PLLR: 96.1097 MHz
mww 0xfffffc2c 0x00481c0e
sleep 10
# PMC_MCKR : MCK = PLL / 2 ~= 48 MHz
mww 0xfffffc30 0x00000007
sleep 10
# MC_FMR: flash mode (FWS=1,FMCN=60)
mww 0xffffff60 0x003c0100
sleep 100
}
$_TARGETNAME configure -work-area-virt 0 -work-area-phys 0x00200000 -work-area-size 0x4000 -work-area-backup 0
#flash bank <driver> <base> <size> <chip_width> <bus_width>
flash bank at91sam7 0 0 0 0 0
# For more information about the configuration files, take a look at:
# openocd.texi
then I connect via telnet to 4444 port
I run the following commands
> arm7_9 dcc_downloads enable
dcc downloads are enabled
> arm7_9 fast_memory_access enable
fast memory access is enabled
> flash write_image erase firmware.bin 0x100000 bin
auto erase enabled
wrote 44616 byte from file firmware.bin in 11.045264s (3.944705 kb/s)
openocd (both r1836 and r1938) are configured using first bootstrap and ./configure --enable-ft2232_libftdi --disable-werror --enable-maintainer-mode
debug trace is too long to attatch.
what is wrong? How can I speed up the process?
Maybe the opensource libftdi? Do I need to try with ftd2xx driver provided by Amontec? I don’t think that is for 64bit systems, isn’t it?
thanks