Hi all,
I use openocd-0.4.0 to download flash program on at91sam7x micro.
My system is ACER Aspire M5641 (intel Q8300 2.5GHz, 4BG ram, Chipset Nvidia MCP73PV), ubuntu linux 9.10 karmic koala x86_64.
Openocd is configured as follows:
./configure --enable-ft2232_libftdi --enable-jlink
I tried with both Amontec jtagkey-tiny and segger j-link
with Amontec jtagkey-tiny I obtain:
Open On-Chip Debugger 0.4.0 (2010-02-25-16:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.berlios.de/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain
Warn : use 'at91sam7s.cpu' as target identifier, not '0'
Info : clock speed 6000 kHz
Info : JTAG tap: at91sam7s.cpu tap/device found: 0x3f0f0f0f (mfg: 0x787, part: 0xf0f0, ver: 0x3)
Info : Embedded ICE version 1
Info : at91sam7s.cpu: hardware has 2 breakpoint/watchpoint units
Info : accepting 'telnet' connection from 0
dcc downloads are enabled
fast memory access is enabled
wrote 51012 bytes from file ../images/DCellEVB.bin in 5.657477s (8.805 kb/s)
and with Segger J-Link:
Open On-Chip Debugger 0.4.0 (2010-02-25-16:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.berlios.de/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain
Warn : use 'at91sam7s.cpu' as target identifier, not '0'
Info : J-Link initialization started / target CPU reset initiated
Info : J-Link compiled Feb 20 2006 18:20:20 -- Update --
Info : JLink caps 0x3
Info : JLink hw version 30000
Info : Vref = 3.233 TCK = 1 TDI = 1 TDO = 1 TMS = 1 SRST = 0 TRST = 255
Info : J-Link JTAG Interface ready
Info : RCLK (adaptive clock speed)
Info : JTAG tap: at91sam7s.cpu tap/device found: 0x3f0f0f0f (mfg: 0x787, part: 0xf0f0, ver: 0x3)
Info : Embedded ICE version 1
Info : at91sam7s.cpu: hardware has 2 breakpoint/watchpoint units
Info : accepting 'telnet' connection from 0
target state: halted
target halted in ARM state due to debug-request, current mode: Supervisor
cpsr: 0x200000d3 pc: 0x00101ce0
dcc downloads are enabled
fast memory access is enabled
wrote 51012 bytes from file ../images/DCellEVB.bin in 4.866550s (10.236 kb/s)
openocd uses the following library
max@lab7:~$ ldd /usr/local/bin/openocd
linux-vdso.so.1 => (0x00007fff351ff000)
libdl.so.2 => /lib/libdl.so.2 (0x00007fc7aaa1f000)
libftdi.so.1 => /usr/local/lib/libftdi.so.1 (0x00007fc7aa818000)
libusb-0.1.so.4 => /usr/local/lib/libusb-0.1.so.4 (0x00007fc7aa613000)
libc.so.6 => /lib/libc.so.6 (0x00007fc7aa2a4000)
/lib64/ld-linux-x86-64.so.2 (0x00007fc7aac23000)
libusb-1.0.so.0 => /lib/libusb-1.0.so.0 (0x00007fc7aa097000)
librt.so.1 => /lib/librt.so.1 (0x00007fc7a9e8f000)
libpthread.so.0 => /lib/libpthread.so.0 (0x00007fc7a9c73000)
I use new version of libusb (v1.0) that should be faster.
That very poor performace are also achieved in debugging ![]()
How can I speed up the flash dowloading?
I read about performace benchmark with openocd:
Openocd r657 with ftdi FT2232 based interface can download @ 26KB/s, and J-link more than 286 KB/s
on amontec site I read about jtagkey-tiny is claimed 125-135kBytes/sec, while jtagkey2 is claimed 525-750kBytes/sec!!! :shock:
So why I can obatin a tenth of that perormance?
I read about Olimex ARM-USB-TINY-H which use usb 2.0 and is clocked @ 30MHz. Is that supported by openocd
thanks