uboot breakpoint in
static void mxc_serial_setbrg(void)
r0 0x0
r1 0x38400
r2 0x0
r3 0x38400
r4 0x0
r5 0x1
r6 0x93ff34
r7 0x0
r8 0x1
r9 0x93fde8
r10 0x0
r11 0x93fdac
r12 0xfffffffd
sp 0x93fd98
lr 0x12054370
pc 0x1205438c
cpsr 0x200001d3
sp_usr 0x0
lr_usr 0x0
r8_fiq 0x0
r9_fiq 0x0
r10_fiq 0x0
r11_fiq 0x0
r12_fiq 0x0
sp_fiq 0x0
lr_fiq 0x0
sp_irq 0x0
lr_irq 0x0
sp_svc 0x93fd98
lr_svc 0x12054370
sp_abt 0x0
lr_abt 0x0
sp_und 0x0
lr_und 0x0
spsr_fiq 0x80a4210
spsr_irq 0x28000b30
spsr_svc 0x42042792
spsr_abt 0x4012516
spsr_und 0xc00ec2b8
sp_mon 0x0
lr_mon 0x0
spsr_mon 0xe60003a0
///////////
openocd
static int target_read_buffer_default(struct target *target, uint32_t address, uint32_t count, uint8_t *buffer)
address=0x93fd80
count=0x40
buffer get:
ACFD9300 70430512 C87C0812 00840300
00000000 00840300 01000000 00B4C404
0A000000 00000000 B4FD9300 44420512
BCFD9300 54450512 C4FD9300 20420512
////////
my uboot map
http://www.mediafire.com/download/6z511 … System.map
prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-gdb will always request openocd return value
add memset(buffer+60,0,4); will remove this error looping
anybody help me C4FD9300 20420512 whats it mean?