I have a RED-V Thing Plus (DEV-15799) that I’m tryong to get working with OpenOCD (v0.11.0). In particular, I want to use telnet to talk to OpenOCD which is turn talks via USB and JLink to the RED-V Thing Plus. I have this mostly working but not completely and I believe the problem is in the OpenOCD “.cfg” files. Are there a set of OpenOCD configuration files (along with the command line that invokes OpenOCD) that are known to work with RED-V Thing Plus?
Could not fund any OpenOCD config files for Red-V thing plus. Hope team sparkfun will look into this matter and provide a feasible solution.
Yes, I hope so too. In the meantime and with the aid of the openocd manual, I’m working on the problem myself. Thank you for your effort.