Openocd debugger set up for M4 core

Hi, I have a program that runs the ARM M4 core on stm32MP157D-DK1 and am trying to debug it with openocd and here is my script

source [find interface/stlink.cfg]
source [find target/stm32mp15x.cfg]
adapter speed 950
gdb_port disabled
stm32mp15x.cpu0 configure -gdb-port disabled
stm32mp15x.cpu1 configure -gdb-port disabled
targets stm32mp15x.cm4
stm32mp15x.cm4 configure -gdb-port 3334
init
halt

Info : [stm32mp15x.cm4] external reset detected
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted

The debugger doesn’t work because M4 cannot be halted no matter what. Could someone please explain why the error exists (script or hardware problem) and how should I adjust my script to run my debugger? Thanks!

This is bit out of my depth, but I kicked this to a few AI models and they had some suggestions
Claude
Perplexity

I ran into the same issues. I got it working by using the CLI tools that STM provides for their devices instead.

They have a custom OpenOCD server:
C:\ST\STM32CubeCLT_1.18.0\STLink-gdb-server\bin\ST-LINK_gdbserver.exe -cp C:\ST\STM32CubeCLT_1.18.0\STM32CubeProgrammer\bin\ -d -m 2 -l 31

And debugger:
C:\ST\STM32CubeCLT_1.18.0\GNU-tools-for-STM32\bin\arm-none-eabi-gdb.exe

1 Like