openOCD flash write_image error(-304)

Hello all,

I am using openOCD 0.4.0. The things that I have is below;

Eclipse IDE,(helios)

A lpc2148 cpu board(uni-ds3 board from mikroelektronika),

ARM-USB-OCD (Olimex) JTAG dongle

all the steps like this;

1- First of all the board can be programmed by using openOCD4.0 with the eclipse.

2- And everythins are ok.

3- When the Hex code transferred to the board again, im getting following error from the console in eclipse.


Open On-Chip Debugger 0.4.0 (2010-02-22-19:05)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.berlios.de/doc/doxygen/bugs.html

500 kHz

RCLK - adaptive

jtag_nsrst_delay: 200

jtag_ntrst_delay: 200

trst_and_srst srst_pulls_trst srst_gates_jtag trst_push_pull srst_open_drain

Info : RCLK (adaptive clock speed) not supported - fallback to 500 kHz

Error: JTAG scan chain interrogation failed: all ones

Error: Check JTAG interface, timings, target power, etc.

error: -100


And the board can not be programmed again…

If i use openOCD + Telnet ,i am getting error again below;


Open On-Chip Debugger

init

reset

JTAG scan chain interrogation failed: all ones

Check JTAG interface, timings, target power, etc.

error: -100

Command handler execution failed

in procedure ‘reset’ called at file “command.c”, line 650

called at file “command.c”, line 361

flash protect 0 0 0 off

cleared protection for sectors 0 through 0 on flash bank 0

flash banks

#0: lpc2000 at 0x00000000, size 0x0007d000, buswidth 0, chipwidth 0

flash erase_sector 0 0 0

Target not halted

failed erasing sectors 0 to 0 (-304)

flash write_image main.hex 0 ihex

Target not halted

error writing to flash at address 0x00000000 at offset 0x00000000 (-304)

Command handler execution failed

in procedure ‘flash’ called at file “command.c”, line 650

called at file “command.c”, line 361


The config file is below;


Olimex ARM-USB-OCD

http://www.olimex.com/dev/arm-usb-ocd.html

interface ft2232

ft2232_device_desc “Olimex OpenOCD JTAG”

ft2232_layout olimex-jtag

ft2232_vid_pid 0x15ba 0x0003

#daemon configuration

telnet_port 4444

gdb_port 3333

jtag speed

jtag_khz 500

Use RCLK. If RCLK is not available fall back to 500kHz.

Depending on cabling you might be able to eek this up to 2000kHz.

jtag_rclk 500

if { [info exists CHIPNAME] } {

set _CHIPNAME $CHIPNAME

} else {

set _CHIPNAME lpc2148

}

if { [info exists ENDIAN] } {

set _ENDIAN $ENDIAN

} else {

set _ENDIAN little

}

if { [info exists CPUTAPID ] } {

set _CPUTAPID $CPUTAPID

} else {

set _CPUTAPID 0x4f1f0f0f

}

jtag_nsrst_delay 200

jtag_ntrst_delay 200

NOTE!!! LPCs need reset pulled while RTCK is low. 0 to activate

JTAG, power-on reset is not enough, i.e. you need to perform a

reset before being able to talk to the LPC2148, attach is not possible.

reset_config trst_and_srst srst_pulls_trst

jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID

set _TARGETNAME $_CHIPNAME.cpu

target create $_TARGETNAME arm7tdmi -endian $_ENDIAN -chain-position $_TARGETNAME -variant arm7tdmi-s_r4

$_TARGETNAME configure -work-area-phys 0x40000000 -work-area-size 0x4000 -work-area-backup 0

$_TARGETNAME configure -event reset-init {

Force target into ARM state

arm core_state arm

Do not remap 0x0000-0x0020 to anything but the flash (i.e. select

“User Flash Mode” where interrupt vectors are not remapped,

and reside in flash instead).

See section 7.1 on page 32 (“Memory Mapping control register”) in

“UM10139: Volume 1: LPC214x User Manual”, Rev. 02 – 25 July 2006.

http://www.standardics.nxp.com/support/ … pc2148.pdf

mwb 0xE01FC040 0x01

disable watchdog

mww 0xfffffd44 0x00008000

enable user reset

mww 0xfffffd08 0xa5000001

CKGR_MOR : enable the main oscillator

mww 0xfffffc20 0x00000601

sleep 10

CKGR_PLLR: 96.1097 MHz

mww 0xfffffc2c 0x00481c0e

sleep 10

PMC_MCKR : MCK = PLL / 2 ~= 48 MHz

mww 0xfffffc30 0x00000007

sleep 10

MC_FMR: flash mode (FWS=1,FMCN=60)

mww 0xffffff60 0x003c0100

sleep 100

}

#flash config komutu

flash bank lpc2000 0 0 <target#> [calc_checksum]

set _FLASHNAME $_CHIPNAME.flash

flash bank $_FLASHNAME lpc2000 0x0 0x7d000 0 0 $_TARGETNAME lpc2000_v2 12000 calc_checksum

init_reset halt

write file to flash memory

arm7_9 dcc_downloads enable

sleep 10

#start execution of the program just downladed

#reset run

#sleep 10

init

reset halt

#flash write_image

flash write_image erase unlock main.hex 0x0 ihex

sleep 10

#exit OpenOCD

shutdown


Where is the mistake??

Best Regards

kamil