OpenOCD on Linux

Hello to everybody, I’m using OpenOCD on Linux with a Wiggler and it works well. What about the other alternatives that are documented to work well on Windows? For example, I know JTAGKey works on Linux because on their site there are the drivers, but what about Signalyzer, ARM-USB-OCD and others? Anyone who used them on Linux, please post its experience. Thanks in advance,

l3golas

Hi,

I use OpenOCD + ARM-USB-OCD and it seems to work fine for me…

Cheers,

–David Carne

All FT2232 based dongles work, and are actually easier to use, because on Linux there’s no need for different drivers for the various VID/PID combinations. Just get the latest version of libftdi or FTDI’s FTD2XX and you should be fine.

All the Wiggler style dongles (‘jtag_interface parport’) work on Linux, as well as Amontec’s JTAG Accelerator, either using direct I/O accesses (requiring root) or using ppdev (/dev/parportN).

The only dongle that wouldn’t work on Linux is the unofficial support for Segger’s J-Link posted to this forum, which is for this reason unlikely to be merged into OpenOCD’s mainline.

Regards,

Dominic

l3golas:
Hello to everybody, I’m using OpenOCD on Linux with a Wiggler and it works well. What about the other alternatives that are documented to work well on Windows?

l3golas

I like to run linux under VMWare with XP as a host OS. openocd runs fine with an FTDI based JTAG dongle redirected to the VMWare session. This lets me run all the windows only garbage I need, and all the linux stuff I like without too much trouble. It takes a decent machine to do well, but it’s not a bad setup.