Hello,
I have installed OpenOCD on my Mac OSX using brew install [–HEAD] openocd
However, when I run ./openocd -f board/st_nucleo_f401re.cfg, I get errors that the specified debug interface was not found. Was openOCD compiled on my machine without stlink support? If so, is it possible to enforce openOCD stlink support during brew install process compilation (the --HEAD option)?
This is the error I get when I run ./openocd -f board/st_nucleo_f401re.cfg:
Open On-Chip Debugger 0.9.0-dev-snapshot (2014-06-13-23:19)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Error: The specified debug interface was not found (hla)
The following debug interfaces are available:
1: dummy
2: jtag_vpi
3: buspirate
4: remote_bitbang
Runtime Error: /usr/local/Cellar/open-ocd/HEAD/share/openocd/scripts/interface/stlink-v2-1.cfg:5:
in procedure ‘script’
at file “embedded:startup.tcl”, line 58
at file “/usr/local/Cellar/open-ocd/HEAD/share/openocd/scripts/board/st_nucleo_f401re.cfg”, line 4
in procedure ‘interface’ called at file “/usr/local/Cellar/open-ocd/HEAD/share/openocd/scripts/interface/stlink-v2-1.cfg”, line 5