I am new to both STM32F3 as well as Open OCD.
I have been following the tutorial on this
http://engineering-diy.blogspot.in/2012 … 0180092033
to setup eclipse as well as open ocd.
I downloaded OpenOCD from sourceforge, built it and installed.
Now when I run the command
openocd -f /usr/local/share/openocd/scripts/board/stm32f3discovery.cfg
Open On-Chip Debugger 0.7.0 (2013-12-11-08:35)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Error: The specified debug interface was not found (hla)
The following debug interfaces are available:
Runtime Error: /usr/local/share/openocd/scripts/interface/stlink-v2.cfg:5:
in procedure ‘script’
at file “embedded:startup.tcl”, line 58
at file “/usr/local/share/openocd/scripts/board/stm32f3discovery.cfg”, line 4
in procedure ‘interface’ called at file “/usr/local/share/openocd/scripts/interface/stlink-v2.cfg”, line 5
On Open OCD bug list there is a bug complaining about stlink not enabled during compile time
http://sourceforge.net/apps/trac/openocd/ticket/66
Is there a work around or a patch for me to get going?