Hi,
For past three days I’m trying to make STM32F0DISCOVERY board (supported in dev version) to work on Linux without success.
Whatever I’m making I always end-up with following error (-d 1):
Debug: 162 14 stlink_usb.c:1145 stlink_usb_open(): stlink_usb_open
Debug: 163 14 stlink_usb.c:1160 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3748
Debug: 164 20 stlink_usb.c:419 stlink_usb_version(): STLINK v2 JTAG v15 API v2 SWIM v0 VID 0x0483 PID 0x3748
Debug: 165 22 stlink_usb.c:561 stlink_usb_init_mode(): MODE: 0x02
Debug: 166 25 stlink_usb.c:593 stlink_usb_init_mode(): MODE: 0x01
Debug: 167 27 stlink_usb.c:372 stlink_usb_error_check(): status error: 9 ('unknown')
Error: 168 27 stlink_usb.c:1241 stlink_usb_open(): init mode failed
Debug: 169 27 stlink_layout.c:50 stlink_layout_open(): failed
Debug: 170 27 command.c:628 run_command(): Command failed with error code -4
Board works perfectly on Windows and Keil enviroment, however I need to run this on Linux.
I’ve check permissions in /dev, different builds from past, hell I even build openocd with libusb on Windows 7 
Error was exactly the same.
Anyone have idea what might be wrong ??
Thanks in advance 
Regards,
You’re using 0.6.0 then? Sorry, I’ve not seen anything like those particular errors. It is mostly working on my Linux Mint install. I’ll paste in the openocd.cfg I’m using. I think most of the weirdness is because I tried to keep 0.5.0 as the default. Not sure though.
set LIBD060 /home/hfs2/local/share/openocd/scripts
## source [find board/stm32f4discovery.cfg]
# source ${LIBD060}/board/stm32f4discovery.cfg
source ${LIBD060}/interface/stlink-v2.cfg
# source ${LIBD060}/target/stm32f4x_stlink.cfg
#
# STM32f4x stlink pseudo target
#
set CHIPNAME stm32f4x
set CPUTAPID 0x2ba01477
set WORKAREASIZE 0x10000
# source [find target/stm32_stlink.cfg]
source ${LIBD060}/target/stm32_stlink.cfg
# stm32f4x family uses stm32f2x driver
set _FLASHNAME $_CHIPNAME.flash
flash bank $_FLASHNAME stm32f2x 0 0 0 0 $_TARGETNAME
gdb_port 3333
telnet_port 4444
tcl_port 8765
As I said, mostly working. OpenOCD seems to work ok via the telnet interface. I can’t remember now the exact nature of the problems I was having - I think it had to do with being able to stop at a breakpoint after reset via gdb.
Lately I’ve been using the [gdbserver and flash utility supplied by [the ST team?]. I do miss some of the telnet features of OpenOCD but the interface to gdb seems more stable.](GitHub - stlink-org/stlink: Open source STM32 MCU programming toolset)
What version of firmware on STLINK device you have ?
What I noticed is that stlink you mentioned also doesn’t work and it worked in past.
The only difference is that I made firmware upgrade to STLINK on windows. Previous one was V14 now it it V15, and I believe that might be connected to my problem.
Does anyone can check what firmware version they have on STM32F0DISCOVERY board STLINK interface ?
This can be seen on debug when openocd is run with “-d 1” option:
Debug: 164 19 stlink_usb.c:419 stlink_usb_version(): STLINK v2 JTAG v15 API v2 SWIM v0 VID 0x0483 PID 0x3748
Maybe there were some changes made by STM and OpenOCD doesn’t work with latest release ?
I would like to know if someone is successfuly using OpenOCD with firmware “v15”, to rule out this posibility.
v14 for me. I completely missed the reference to -d 1 in your first post. Lots of output!
Debug: 162 33 stlink_layout.c:43 stlink_layout_open(): stlink_layout_open
Debug: 163 33 stlink_usb.c:1005 stlink_usb_open(): stlink_usb_open
Debug: 164 33 stlink_usb.c:1020 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3748
Debug: 165 113 stlink_usb.c:413 stlink_usb_version(): STLINK v2 JTAG v14 API v2 SWIM v0 VID 0x0483 PID 0x3748
Debug: 166 115 stlink_usb.c:555 stlink_usb_init_mode(): MODE: 0x02
Debug: 167 118 stlink_usb.c:587 stlink_usb_init_mode(): MODE: 0x01
Debug: 168 121 stlink_usb.c:620 stlink_usb_init_mode(): MODE: 0x02
Debug: 169 121 stlink_interface.c:53 stlink_interface_init_target(): stlink_interface_init_target
Debug: 170 123 stlink_usb.c:647 stlink_usb_idcode(): IDCODE: 0x2BA01477
Debug: 171 123 openocd.c:145 handle_init_command(): Examining targets...
Debug: 172 123 arm_adi_v5.c:1097 ahbap_debugport_init():
Debug: 173 123 arm_adi_v5.c:1103 ahbap_debugport_init(): No low level jtag hardware found
Debug: 174 123 stm32_stlink.c:631 stm32_stlink_read_memory(): stm32_stlink_read_memory 0xe000ed00 4 1
Debug: 175 125 target.c:1908 target_read_u32(): address: 0xe000ed00, value: 0x410fc241
Debug: 176 125 cortex_m.c:1788 cortex_m3_examine(): Cortex-M4 r0p1 processor detected
Debug: 177 125 cortex_m.c:1789 cortex_m3_examine(): cpuid: 0x410fc241
I have used stlink/v1 and stlink/v2 with both firmware versions v14 and v15.
you still getting problems ?
Spen