openOCD - STM32L082 upload

Hello,

I am playing with the STM32L082 to use the Dual Bank of the flash memory. For that I am using platformio and openOCD.

When programming with OCD I get upload error and info that NVM address of bank2 is not found (see below)

Warn : no flash bank found for address 0x08018000
Warn : no flash bank found for address 0x0801b75c

Any suggestions? I no clue what I am missing here.

CURRENT: upload_protocol = stlink
openocd -d2 -s C:\Users\jeroen\.platformio\packages\tool-openocd/scripts -f board/JENG_STM32L082KZ.cfg -c "program {.pio\build\STM32L082_bank2\firmware.elf}  verify reset; shutdown;"
xPack OpenOCD x86_64 Open On-Chip Debugger 0.11.0+dev (2021-10-16-21:19)
Licensed under GNU GPL v2
For bug reports, read
        http://openocd.org/doc/doxygen/bugs.html
debug_level: 2

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : clock speed 300 kHz
Info : STLINK V2J34S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 1.769585
Info : STM32L082KZTx.cpu: Cortex-M0+ r0p1 processor detected
Info : STM32L082KZTx.cpu: target has 4 breakpoints, 2 watchpoints
Info : starting gdb server for STM32L082KZTx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : Unable to match requested speed 300 kHz, using 240 kHz
Info : Unable to match requested speed 300 kHz, using 240 kHz
target halted due to debug-request, current mode: Thread 
xPSR: 0xf1000000 pc: 0x08002da8 msp: 0x20005000
STM32L0: Enabling HSI16
Info : Unable to match requested speed 2500 kHz, using 1800 kHz
Info : Unable to match requested speed 2500 kHz, using 1800 kHz
** Programming Started **
Info : Device: STM32L0xx (Cat.5)
Info : STM32L flash has dual banks. Bank (0) size is 96kb, base address is 0x8000000
Warn : no flash bank found for address 0x08018000
Warn : no flash bank found for address 0x0801b75c
** Programming Finished **
** Verify Started **
** Verified OK **
** Resetting Target **
Info : Unable to match requested speed 300 kHz, using 240 kHz
Info : Unable to match requested speed 300 kHz, using 240 kHz
in procedure 'program'
*** [upload] Error 1

Hi, did you check this?

https://stackoverflow.com/questions/490 … 0x00000000