OPT4048DTSR incorrect CCT reading

Eh, I just have some general suggestions:

  1. Calibration: The sensor may need proper calibration. The OPT4048 typically requires calibration to account for variations in manufacturing and to adjust for specific light conditions.
  2. Optical considerations:
  • Ensure that the sensor’s aperture is clean and unobstructed.
  • Check if there are any reflective surfaces near the sensor that might affect readings.
  1. Integration time: Adjust the integration time settings. Longer integration times can improve accuracy but may reduce the sensor’s ability to handle rapid changes in light conditions or maybe not be linear across different frequencies.
  2. Gain settings: Verify that the gain settings are appropriate for your light conditions. High gain can improve sensitivity in low-light conditions but may lead to saturation in brighter environments.
  3. Light source characteristics: The type of light source you’re measuring can affect readings. Ensure you’re using the sensor in conditions similar to those it was designed for.
  4. Temperature effects: The OPT4048 can be sensitive to temperature changes. Ensure the sensor is operating within its specified temperature range as well.
  5. Power supply stability: Ensure a stable power supply to the sensor, as voltage fluctuations can affect readings.

To address these potential issues:

  1. Review the datasheet and application notes for the OPT4048DTSR for specific calibration procedures.
  2. Experiment with different integration time and gain settings to find the optimal configuration for your use case.
  3. If possible, compare your sensor’s readings with a calibrated reference device to help narrow down/identify discrepancies.