Out of a box solution

I would like to have a complete RTK solution.

I mean the system shall include base station, Rover, radio and (if needed) processing software if I need to work as post processing kinematic.

My target is tens of centimeter accuracy.

Best regards

So, there are a lot of options for this…do you strictly need a base + rover or is using PPP instead a viable route? It’d save quite a bit of cost

If you do need a base + rover, how far apart will they be? Some of our models have bt/wifi/espnow on-board which could also save cost…but if the distance is far lora radios are the longest-reaching

How many tens of cm?

We mostly use/advocate for open source software, I can give you some suggestions: will you be using iOS or android or windows or what?

Thank you so much for your replay.
I will use a base and rover.
The distance mostly will be 1-3 km.
The accuracy is in the range of 10 cm.
The availability of wifi or radio is not granted so i would need a post processing software.
CHEERS

Alrighty! Here’s a list:
2x RTK Board
2x antenna
2x Ground Plane
2x LoRa board
2x LoRa antennae
2x adapters for LoRa

This would provide an accuracy of a few cm and be able to work up to ~6 miles with line-of-sight

Be sure to go through the hookup guide(s) for the RTK boards and LoRa boards and you should be all set!

Thanks a lot for your help and answer.

Can I get that as two assembled receivers?

Which software you recommend for post processing?

If the above is possible, can a get an offer.

Thanks a lot

Sparkfun products are generally intended for experimenters who enjoy putting hardware together and learning how to code and operate it.

For a “complete beginner” plug and play RTK setup, consider buying a set like the rather dated UBlox C94-M8P, and carefully follow the instructions in the box. A few are still available at a reasonable price. I learned a lot, working with mine.

Comprehensive, independent performance review of the product: https://www.calvert.ch/maurice/2017/08/28/ublox-c94-m8p-rtk-gps-review-performance-evaluation/