Pad holes do not show when printing with Eagle

Hi

I have been using Eagle Lite off and on for quite a while. Recently installed 6.1.0 on Windows 7. I always remember when printing the board fro etching the pads holes showed. I need this to hand drill the holes. Now this is not happening. I have looked around for solution and some mentioned that display mode should be set to “real” and it is. One more thing, if I print to file (pdf) the holes show :?: :?:

This seems to be a problem associated with the HP 6P printer. I can print to my inkjet and the holes do show as expected. Unfortunately I must use the HP 6P fro my PCB needs. I loaded a driver for Windows 7 that I got from the HP site and maybe that just isn’t working correctly. On this same computer when running XP I did not have any problem with missing holes. The woraround is to print to a pdf file (this shows the holes) and print the pdf to the HP 6P. This method does show the holes correctly.