I am running into an issue with my Papa Soundie. I am running the example code and the arduino portion seems to be running just fine (outputting serial information to verify), but I am getting nothing but a buzz out of the audio connection. I am using a MicroSD XC card formatted FAT32 and have tried reformatting as well as a whole slew of different audio files in both supported formats.
I’m wondering if there are any known compatibility issues with MicroSD cards classed above standard MicroSD or MicroSD HC. I have two (terribly expensive for what they are) class 10 cards coming from Sparkfun in the hopes this will resolve the issue, but would like to bring forward a potential forward compatibility issue that should be addressed on the product page to ensure no one runs into the same issue if it is indeed known.