Hello,
I have a papa soundie and noisy cricket combined to play an audio file.
My set up is as follows:
Papa Soundie:
VIN and GRND tied into bread board + and -
3.3v bread board power supply on the breadboard.
L and R audio going out to to the Cricket L and R in pins
SD card formatted to FAT32 with one audio file labeled AUDIO00.OGG and is an OGG file from the converter found on the tutorial. Audio file plays fine from the SD card on my laptop when opened.
Used the FTDI to upload the tutorial code that loops the audio files every 5 seconds, upload successfully uploaded,
Cricket:
3.3v and GND tied to bread board + and - respectively
L and R In coming from the soundie
L and MONO out going to the Spark Fun Thin Speaker - 0.5W
Bridged the Mono spot on the back and the mono sub as per the tutorial
Powered everything up and no audio, I have tried multiple example sketches, Ive tried hooking a self powered speaker into the 3.5mm out, The cricket is online and if you touch the pins on the back i can hear feedback at the speaker so i know the volume and speaker are both working.
I am lost as to why i cant get audio going.
Any help would be greatly appreciated.