People,
I DO NOT WANT TO START A FLAME WAR.
I tried to read the other thread, but it got too confusing (and vitriolic) for me.
What is the current state of play with PCB design software?
My first design will be for a board that just under 160mm x 96mm {thus it’s too big for the free version of Eagle).
I have no $ (well none to spend on PCB design software yet - even if I did, the budget would be more like $200 than $2K).
I have looked at a couple of the free packages (ExpressPCB and Pad2PAd) but these seem to be based on going to a particular supplier for manufacture. None of the manufacturer specific packages seem to be able to export the file to anything other than the manufacturer’s web site (So I couldn’t draw up a board, and say, export the Gerber file to the local board etcher).
Most (all?) seem to allow schematics to be done within the same package. This is an excellent feature.
Auto routing is a good bonus, but I wouldn’t be heartbroken if I had to hand route.
Libraries would be nice - I hate having to re-invent the wheel.
I have used AutoCAD over the years, so ‘arcane’ ways of doing things doesn’t particularly scare me {annoy yes, scare no}
Predominately I’m working in Windows XP but would like to move to 100% Linux one day. I run several Vendor specific packages (not wine compatible) so that day is still probably some time aways.
Are there other packages I should be looking at? (AutoCAD with the “design PCB module”?, Microsoft’s “MS-PCBdesigner”?, “super easy PCB designer that does everything for free and makes coffee”?)
Are their other tricks I should try? Draw the schematic in Eagle, and ask nicely if someone would be prepared to place/route the board for me? Get a board manufacturer to design the board based on my schematic?
PLEASE don’t get into a pissing contest with “Mine’s better than yours”.
Thanks in advance…